Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22314
  • Release Date : 2018/08/30 13:55
  • Print

Regarding the settings of built-in analog function of FX5U CPU module

Are there any required settings for using the built-in analog function?
Category : 

Answer

The settings can be done using the parameter settings of GX Works3 or by settings the special relay/special registers.
For further details please refer to MELSEC iQ-F FX5 User's Manual (CPU Module Built-In Analog/Expansion-Adapter).
6 FX5U CPU MODULE BUILT-IN ANALOG
6.7 Parameter Setting
Product Name
FX5U
Product Category
CPU Module, Analog Control
Series
FX5U
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?