Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22317
  • Release Date : 2018/08/30 13:55
  • Update : 2023/06/23 10:19
  • Print

Regarding CC-Link settings using GX Works3

Answer

Parameters can be set when connecting the MELSEC iQ-F series with FX5-CCL-MS(CC-Link system master/intelligent device).
However, when connecting with FX3U-16CCL-M(CC-Link master), the settings must be configured using a program.
For further details, please refer to the example programs in FX3U-16CCL-M User's Manual
Product Name
FX3U-16CCL-M, FX5-CCL-MS
Product Category
CPU Module, Network/Communication, Engineering Software
Series
MELSEC iQ-F シリーズ

May I have your opinion?

Inquiries