FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Engineering Software > Regarding CC-Link settings using GX Works3
FAQ
Regarding CC-Link settings using GX Works3
Is it possible to set the CC-Link settings through the parameter settings of GX Works3?
- Category :
-
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Engineering Software
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Network/Communication
Answer
Parameters can be set when connecting the MELSEC iQ-F series with FX5-CCL-MS(CC-Link system master/intelligent device).
However, when connecting with FX3U-16CCL-M(CC-Link master), the settings must be configured using a program.
For further details, please refer to the example programs in FX3U-16CCL-M User's Manual
However, when connecting with FX3U-16CCL-M(CC-Link master), the settings must be configured using a program.
For further details, please refer to the example programs in FX3U-16CCL-M User's Manual
- Product Name
- FX3U-16CCL-M, FX5-CCL-MS
- Product Category
- CPU Module, Network/Communication, Engineering Software
- Series
- MELSEC iQ-F シリーズ