FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding the cause of communication error with GX Works3
FAQ
Regarding the cause of communication error with GX Works3
The communication between GX Works3 and MELSEC iQ-F Series via Ethernet connection could not be enabled. What is the possible cause?
Answer
From the PC's Internet Protocol Version 4 Properties, uncheck "Obtain an IP address automatically" option
and set an arbitrary IP adress that does not duplicate with the address of FX5-CPU module.
Also, if the subnet mask is 255.255.255.0, the first three values (first - third octets) must match the FX5-CPU module's IP address.
*The default IP address of FX5-CPU module is 192.168.3.250 and 255.255.255.0 for subnet mask.
As well, the security softwares (antivirus software) may be blocking the Ethernet communication.
Check if communication is enabled by temporarily disabling the security software or by authorizing communication through the security software settings.
and set an arbitrary IP adress that does not duplicate with the address of FX5-CPU module.
Also, if the subnet mask is 255.255.255.0, the first three values (first - third octets) must match the FX5-CPU module's IP address.
*The default IP address of FX5-CPU module is 192.168.3.250 and 255.255.255.0 for subnet mask.
As well, the security softwares (antivirus software) may be blocking the Ethernet communication.
Check if communication is enabled by temporarily disabling the security software or by authorizing communication through the security software settings.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Engineering Software
- Series
- MELSEC iQ-F Series