FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the specifications of the built-in Ethernet function of FX5 CPU module
FAQ
Regarding the specifications of the built-in Ethernet function of FX5 CPU module
What is the maximum number of connections that can be made using the built-in Ethernet port?
Answer
The connection using the Ethernet port can establish a total of 8 connections which includes SLMP, MELSOFT connection, MODBUS/TCP, socket communication, and predefined protocol support function.
The first of MELSOFT(connection with GX Works3) connection, CC-Link IE field network Basic, FTP server, SNTP client, and Web server page are not included in the number of connections.
For details, please refer to
MELSEC iQ-F FX5 User's Manual (Communication)
The first of MELSOFT(connection with GX Works3) connection, CC-Link IE field network Basic, FTP server, SNTP client, and Web server page are not included in the number of connections.
For details, please refer to
MELSEC iQ-F FX5 User's Manual (Communication)
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series