FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Network/Communication > Regarding expansion of communication ports
FAQ
Regarding expansion of communication ports
Is is possible to add communication port to FX5 CPU module and use the MODBUS communication on multiple communication channels?
Answer
MODBUS serial communication over multiple communication channels is possible.
The MODBUS serial communication settings can be set from GX Works3 parameters.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series