Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22324
  • Release Date : 2018/08/30 13:55
  • Print

Regarding the maximum number of connections for MODBUS communication

When MODBUS communication is used as master station, how many slave stations can be connected?
Category : 

Answer

32 stations can be connected when RS-485 port is used and only 1 station can be connected when RS-232 port is used.
Product Name
FX5U, FX5UC
Product Category
CPU Module, Network/Communication
Series
MELSEC iQ-F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?