- No : 22329
- Release Date : 2018/08/30 13:55
-
Print
Regarding the latch settings of data register
When FX5U/FX5UC CPU module's power is set to OFF, data register(D100) is cleared.
Are there any settings required to latch this register?
- Category :
-
Answer
It is necessary to set the latch range from the following GX Works3 parameters:
[Navigation Window] -> [CPU Parameters] -> [Device/Memory Settings] -> [Device/Label Memory Area Setting]
- Product Name
- FX5U, FX5UC
- Product Category
- CPU Module, Engineering Software, GX Works3
- Series
- MELSEC iQ-F Series