FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Communication between CPUs via built-in Ethernet port in LCPU
FAQ
Communication between CPUs via built-in Ethernet port in LCPU
Which communication methods are available between CPUs via the built-in Ethernet port in the L series CPU?
- Category :
Answer
The following communication methods are available between the built-in Ethernet ports in the L series CPUs.
- Simple PLC communication function
- Socket communication function
- Simple PLC communication function
- Socket communication function
- Product Name
- MELSEC-L Series
- Series
- L Series