FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Connection status detection between a hub and the built-in Ethernet port of LCPU
FAQ
Connection status detection between a hub and the built-in Ethernet port of LCPU
Is there any method to know the connection status between the built-in Ethernet port in the L series CPU and a hub?
- Category :
Answer
The bit 10 of the special register SD1288 provides the connection status to a hub. When the bit 10 of SD1288 is ON, a hub is connected.
- Product Name
- MELSEC-L Series
- Series
- L Series