FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Difference between standard inputs A06 to B11 and high-speed inputs A12 to B20 of LCPU built-in I/O function
FAQ
Difference between standard inputs A06 to B11 and high-speed inputs A12 to B20 of LCPU built-in I/O function
When using the LCPU built-in I/O function, what are differences between connecting to the standard inputs A06 to B11 and to the high-speed inputs A12 to B20 ?
- Category :
Answer
The minimum input response times are different. The minimum input response time is 100 microseconds for standard inputs, and 10 microseconds for high-speed inputs, allowing high speed response.
- Product Name
- MELSEC-L Series
- Series
- CPU