FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Using send FBs/receive FBs simultaneously
FAQ
Using send FBs/receive FBs simultaneously
Is it possible to execute multiple send FBs/receive FBs created using GX Configurator-SC simultaneously for sending/receiving?
- Category :
Answer
If multiple send FBs/receive FBs are simultaneously executed, the FBs do not function properly.
When there are multiple send FBs, do not execute two or more send FBs simultaneously. (Create a program that does not turn ON the I_START instructions for the send FBs simultaneously.)
When there are multiple receive FBs, do not execute two or more receive FBs simultaneously. (Create a program that does not turn ON the I_START instructions for the receive FBs simultaneously.)
When there are multiple send FBs, do not execute two or more send FBs simultaneously. (Create a program that does not turn ON the I_START instructions for the send FBs simultaneously.)
When there are multiple receive FBs, do not execute two or more receive FBs simultaneously. (Create a program that does not turn ON the I_START instructions for the receive FBs simultaneously.)
- Product Name
- Engineering Software
- Series
- Software Package (other functions)