Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23032
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/27 12:14
  • Print

CC-Link IE Controller cable standard

What are the notes for buying commercial optical cables (type of cable and connector, number of cores, core diameter, cladding diameter, etc.)?
Category : 

Answer

Use the cables that meet the IEC60793-2-10 Types A1a.1 optical fiber standard. The connectors are LC (duplex) connectors.
Two cores are required.The core diameter is 50 [um] and the cladding diameter is 120 [um].
Product Name
Network Related Products
Series
CC-Link IE Controller Network

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries