FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > CC-Link IE Controller cable standard
FAQ
CC-Link IE Controller cable standard
What are the notes for buying commercial optical cables (type of cable and connector, number of cores, core diameter, cladding diameter, etc.)?
- Category :
Answer
Use the cables that meet the IEC60793-2-10 Types A1a.1 optical fiber standard. The connectors are LC (duplex) connectors.
Two cores are required.The core diameter is 50 [um] and the cladding diameter is 120 [um].
Two cores are required.The core diameter is 50 [um] and the cladding diameter is 120 [um].
- Product Name
- Network Related Products
- Series
- CC-Link IE Controller Network