Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23051
  • Release Date : 2018/09/03 17:31
  • Update : 2019/06/27 15:46
  • Print

Cascade connections between hubs in the CC-Link IE Field Network

Is there a limitation on the number of levels of the cascade connections between hubs?
Category : 

Answer

UP to 20 levels of cascade connections can be made.
Product Name
Network Related Products
Series
CC-Link IE Field Network
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?