FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Precaution about MELSECNET/H connection (1)
FAQ
Precaution about MELSECNET/H connection (1)
What are the precautions for connecting a Q series redundant system using the MELSECNET/H PLC to PLC network system?
- Category :
Answer
- Set successive station numbers for the network modules in system A and system B in a redundant system.
(Station number 0 cannot be set.)
- Match "host's send range" for the network module in system A with that in system B.
The pairing setting is provided to match "host's send range" for the network modules in system A and B.
For the control station in a network system including a redundant system, make the pairing setting for the network modules
in system A and B using the Network Parameter setting.
(Station number 0 cannot be set.)
- Match "host's send range" for the network module in system A with that in system B.
The pairing setting is provided to match "host's send range" for the network modules in system A and B.
For the control station in a network system including a redundant system, make the pairing setting for the network modules
in system A and B using the Network Parameter setting.
- Product Name
- Network Related Products
- Series
- MELSECNET/H