FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding clearing error with SM50
FAQ
Regarding clearing error with SM50
Does turning on SM50 clear the error code stored in SD0?
Answer
It is cleared by eliminating the cause of the error during detection and turning on SM50.
For the error codes that can be cleared on the SM50, refer to the manual below.
MELSEC iQ-F FX5 User's Manual (Application)
For the error codes that can be cleared on the SM50, refer to the manual below.
MELSEC iQ-F FX5 User's Manual (Application)
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series