FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding the requirement of SD Memory Card module function of FX5S CPU module
FAQ
Regarding the requirement of SD Memory Card module function of FX5S CPU module
Does the FX5S CPU unit have any functions that require an SD memory card module: FX5-SDCD?
Answer
SD Memory Card Module: FX5-SDCD is required for the following functions.
・Firmware update function ※ 1
・Memory card function (SD memory card forced stop, boot operation)
・Data logging function
・Memory dump function
・Backup/Restore
・File transfer function (FTP server)
・File transfer function (FTP client)
・Web server functions (user web pages)
・Firmware update function ※ 1
・Memory card function (SD memory card forced stop, boot operation)
・Data logging function
・Memory dump function
・Backup/Restore
・File transfer function (FTP server)
・File transfer function (FTP client)
・Web server functions (user web pages)
※1 The firmware of FX5S CPU module can be updated using engineering tool. By updating the firmware from the engineering tool, it is possible to update the firmware without using the SD memory card module or SD memory card.
- Product Name
- FX5S
- Product Category
- CPU Module, Option
- Series
- MELSEC iQ-F Series