FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding differences in specifications of the FTP server auto transfer function for data logging files
FAQ
Regarding differences in specifications of the FTP server auto transfer function for data logging files
Is there any difference in the FTP server auto transfer function between the iQ-F series and the iQ-R series?
Answer
The following points are different for the iQ-F series.
・Error History
If the FX5 CPU Module is turned off, the error history is cleared.
・Setting details of the CPU Module Logging Configuration Tool
DNS server settings are not supported.
・Directory
If the specified directory does not exist on the FTP server, no error occurs and the directory is created and the file is transferred.
・Error History
If the FX5 CPU Module is turned off, the error history is cleared.
・Setting details of the CPU Module Logging Configuration Tool
DNS server settings are not supported.
・Directory
If the specified directory does not exist on the FTP server, no error occurs and the directory is created and the file is transferred.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series