Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 44361
  • Release Date : 2024/03/27 15:55
  • Print

Regarding swapping upper and lower bytes of string data

If the device where the character string is stored: D0~ is displayed in GOT, "3412" is displayed. Is there an instruction to swap the upper and lower bytes of a string?
Category : 

Answer

You can use the SWAP (P) command to swap the upper and lower bytes of the specified device.
Product Name
FX5U,FX5UC,FX5UJ,FX5S
Product Category
CPU Module, Engineering Software
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries