FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Engineering Software > Regarding swapping upper and lower bytes of string data
FAQ
Regarding swapping upper and lower bytes of string data
If the device where the character string is stored: D0~ is displayed in GOT, "3412" is displayed. Is there an instruction to swap the upper and lower bytes of a string?
Answer
You can use the SWAP (P) command to swap the upper and lower bytes of the specified device.
- Product Name
- FX5U,FX5UC,FX5UJ,FX5S
- Product Category
- CPU Module, Engineering Software
- Series
- MELSEC iQ-F Series