FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding compatible version of CANopen communication function for PDO communication
FAQ
Regarding compatible version of CANopen communication function for PDO communication
When using PDO communication of CANopen communication function with FX5-CCLGN-MS, are there any restrictions on firmware version, etc.?
Answer
It is necessary to use the following CPU module, FX5-CCLGN-MS, GX Works3 versions.
FX5-CCLGN-MS・・・1.020 or later
FX5U/FX5UC CPU module ・・・1.260 or later
FX5UJ CPU module ・・・1.070 or later
GX Works3・・・1.105 K or later
FX5U/FX5UC CPU module ・・・1.260 or later
FX5UJ CPU module ・・・1.070 or later
GX Works3・・・1.105 K or later
*If the firmware of the FX5-CCLGN-MS does not support the CANopen communication function, a network error (error code: 2221 H) or initialization failure (event code: 00C54) occurs and the data link will not work.
- Product Name
- FX5-CCLGN-MS
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series