FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Motor: SF-HJCA
FAQ
Motor: SF-HJCA
When connecting the SF-HJCA motor, what should be set in Pr.71 (applied motor)?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > Peripheral devices
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Configure the same setting as the SF-HRCA. Configure the same setting as the SF-HRCA. A700, E700, D700, F700PJ: Pr.71 = 50F700P, F700: Pr.71 = 1 (Reference) SF-HRCA: steel plate frame, SF-HJCA: casting frame (The electrical characteristics are the same.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-D700, FR-E700, FR-F700, FR-F700P, FR-F700PJ