FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-PA07
FAQ
FR-PA07
When using the enclosure surface operation panel FR-PA07, is there any necessary settings?
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
Specific settings are not required, however, when replacing the FR-E500, check that Pr.146 (Built-in potentiometer switchover) is not set to "0".
If it is "0", change it to "1".
If it is "0", change it to "1".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700