Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21366
  • Release Date : 2018/08/22 16:27
  • Print

FR-PA07

How can I disable the dial operation except the frequency setting when using the enclosure surface operation panel FR-PA07?
Category : 

Answer

Operations cannot be enabled separately.

You only can disable or enable all the operations.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries