FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to indication of the measurement value of the electric energy (EcoMonitorPlus/Light).
FAQ
As to indication of the measurement value of the electric energy (EcoMonitorPlus/Light).
What happens when the measurement value of the electric energy exceeds 99999.9kWh(MWh)?
Answer
It measures from 0kWh(MWh) after going round.
Integer 4 digits : 9999.98→9999.99→0000.00→0000.01kWh(MWh)
Integer 5 digits : 99999.8→99999.9→00000.0→00000.1kWh(MWh)
Integer 6 digits : 999998→999999→000000→000001kWh
Integer 4 digits : 9999.98→9999.99→0000.00→0000.01kWh(MWh)
Integer 5 digits : 99999.8→99999.9→00000.0→00000.1kWh(MWh)
Integer 6 digits : 999998→999999→000000→000001kWh
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight
May I have your opinion?
Related FAQ
- Simultaneous data acquisition of MODBUS RTU communication and Optional Unit.
- As to using SD memory card at multiple locations.
- As to logging period of the optional SD memory card (EMU4-SD2GB).
- As to action upon memory shortage of the SD memory card.
- As to timing for outputting data file into the SD memory card.