Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22461
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/18 15:46
  • Print

Using a commercially-available SD memory card for a MELSEC iQ-R series CPU module

Can I use a commercially-available SD memory card for a MELSEC iQ-R series CPU module?
Category : 

Answer

For the commercially-available SD memory cards that can be used for MELSEC iQ-R series CPU modules,
refer to the following technical bulletin.
- TECHNICAL BULLETIN No. FA-A-0078
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?