FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > OS compatible with GX Works3
FAQ
OS compatible with GX Works3
Which OS is compatible with GX Works3?
- Category :
Answer
GX Works3 is compatible with the following OSs. (As of Sep,2018)
- Microsoft Windows 10
- Microsoft Windows 8.1
- Microsoft Windows 8
- Microsoft Windows 7
- Microsoft Windows Vista *
- Microsoft Windows XP *
(* GX Works3 is not compatible with Windows XP or Windows Vista of 64-bit version.)
- Microsoft Windows 10
- Microsoft Windows 8.1
- Microsoft Windows 8
- Microsoft Windows 7
- Microsoft Windows Vista *
- Microsoft Windows XP *
(* GX Works3 is not compatible with Windows XP or Windows Vista of 64-bit version.)
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- Combination of the MELSEC iQ-R series inter-module synchronization function and the fixed scan communication of the multiple CPU system function
- Interrupt program priority setting of MELSEC iQ-R series
- I/O assignment of PLC parameters with GX Works3
- Using Q series terminal blocks and connectors with MELSEC iQ-R series modules
- Database function of the MELSEC iQ-R series