FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > I/O assignment of PLC parameters with GX Works3
FAQ
I/O assignment of PLC parameters with GX Works3
Where can I set the I/O assignment of PLC parameters with GX Works3?
- Category :
Answer
"PC Parameter" in GX Works2 is "Parameter" in GX Works3.
You can set the I/O assignment from "Module Configuration" or "System Parameter".
<Setting from the module configuration>
[Navigation Window] -> [Project] -> [Module Configuration]
<Setting from the system parameter>
[Navigation Window] -> [Parameter] -> [System Parameter] -> [I/O Assignment]
You can set the I/O assignment from "Module Configuration" or "System Parameter".
<Setting from the module configuration>
[Navigation Window] -> [Project] -> [Module Configuration]
<Setting from the system parameter>
[Navigation Window] -> [Parameter] -> [System Parameter] -> [I/O Assignment]
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- How to use the database function of the MELSEC iQ-R series
- How to check the scan time with GX Works3
- Differences between GX Works3 and GX Works2
- Combination of the MELSEC iQ-R series inter-module synchronization function and another network synchronous communication function
- IP filter function of MELSEC iQ-R series CPU modules