Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22479
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/19 15:01
  • Print

IP filter function of MELSEC iQ-R series CPU modules

What is the IP filter function of MELSEC iQ-R series CPU modules?
Category : 

Answer

You can set IP addresses accessible to the CPU module and prevent unauthorized access to the CPU module.

<Setting the IP filter function>
[Navigation Window] -> [Parameter] -> [CPU Module] -> [Module Parameter] -> [Application Setting] -> [Security] -> [IP Filter Settings]
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?