Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22486
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 09:30
  • Print

How to check devices assigned to labels of GX Works3

How can I check devices assigned to local labels of GX Works3?
Category : 

Answer

GX Works3 and the MELSEC iQ-R series do not use actual devices as automatic assignment devices of local labels.
The local labels use "label areas" in the "device/label memory".
You do not have to worry about devices such as when using GX Works2.

<Setting label areas>
Select [Navigation Window] -> [Parameter] -> [CPU Module] -> [CPU Parameter] -> [Memory/Device Setting] 
-> [Device/Label Memory Area Setting] -> [Label Area] and specify the space.
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?