Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22489
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 09:43
  • Print

Differences between GX Works3 and GX Works2

What are the differences between GX Works3 and GX Works2?
Category : 

Answer

GX Works3 provides various intuitive features such as graphic-based system configuration and an extensive
module library (module label/FB) as standard.
You can reduce the time to be taken for programming with GX Works3 by 40% as compared with GX Works2.
(Based on new project test benchmarks between GX Works2 and GX Works3)
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?