FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Number of modules that can be synchronized using the MELSEC iQ-R series inter-module synchronization function
FAQ
Number of modules that can be synchronized using the MELSEC iQ-R series inter-module synchronization function
How may modules can be synchronized using the MELSEC iQ-R series inter-module synchronization function?
- Category :
Answer
The number of modules that can be synchronized is as follows.
- In single CPU system configuration: 64 modules
- In multiple CPU system configuration: 57 to 63 modules
Mounting positions of the modules and the maximum number of mountable modules do not change regardless of whether
the inter-module synchronization function is used or not.
Since RnENCPU occupies two slots, one or more slots are occupied, so the maximum number of installable modules decreases.
- In single CPU system configuration: 64 modules
- In multiple CPU system configuration: 57 to 63 modules
Mounting positions of the modules and the maximum number of mountable modules do not change regardless of whether
the inter-module synchronization function is used or not.
Since RnENCPU occupies two slots, one or more slots are occupied, so the maximum number of installable modules decreases.
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- Inter-module synchronization function of MELSEC iQ-R series
- How to display the parameter setting window for a programmable controller with GX Works3
- Security key authentication function of MELSEC iQ-R series
- Operations that can be performed with the MELSEC iQ-R series inter-module synchronization function
- Processing time of when multiple programs are executed with a MELSEC iQ-R series CPU module