Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22503
  • Release Date : 2018/09/03 17:28
  • Print

Difference between GX Works2 and GX Developer

What are the differences between GX Works2 and GX Developer?
Category : 

Answer

Main differences between GX Works2 and GX Developer are as follows:
-The functions of GX Configurator and GX Simulator are integrated as GX Works2. No additional software is required.
- Compared to GX Developer, the user interface, operability, and functions are improved in GX Works2.
- Compatible CPU modules are different for GX Works2 and GX Developer.

For more details, refer to the following manual.
- GX Works2 Version 1 Operating Manual (Common) Appendix 4
Product Name
Engineering Software
Series
Software Package (GPP function)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?