Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22504
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 13:10
  • Print

USB driver installation

Does a USB driver need to be installed for connecting a personal computer with a QCPU?
Category : 

Answer

Yes. A USB driver needs to be installed.For the installation procedure, refer to the following manual.

- GX Developer Version 8 Operating Manual (Startup)
Product Name
MELSEC-Q Series
Series
Software Package (GPP function)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?