FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Including GX Developer in GX Works2
FAQ
Including GX Developer in GX Works2
Is GX Developer included in GX Works2?
- Category :
Answer
Yes, it does.
GX Developer can be installed along with the installation of GX Works2.
For more details of the installation procedure, refer to GX Works2 Version 1 Operating Manual (Common).
GX Developer can be installed along with the installation of GX Works2.
For more details of the installation procedure, refer to GX Works2 Version 1 Operating Manual (Common).
- Product Name
- MELSEC-Q Series
- Series
- Software Package (GPP function)