Start main contents
HOME
FAQ
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-Q Series
>
Error code "4100" in QCPU
FAQ
/category/show/2486
Edge Computing Products
(20)
/category/show/1993
Controllers
(1616)
/category/show/1995
Programmable Controllers MELSEC
(1202)
MELSEC iQ-R Series
(45)
MELSEC iQ-F Series
(144)
MELSEC-Q Series
(213)
MELSEC-L Series
(105)
MELSEC-F Series
(456)
Network related products
(110)
Engineering Software
(129)
/category/show/1997
Motion Controllers
(414)
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
No : 22533
Release Date : 2018/09/03 17:28
Update : 2018/09/20 14:43
Print
Error code "4100" in QCPU
The error code "4100" is displayed on QCPU.
The instruction in which the error occurs is [D/ D6270 D6268 D6268]. Are there any remedies?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-Q Series
Answer
The error code "4100" is "OPERATION ERROR".
The error occurs when a number is divided by 0 (Divisor D6268 value is 0).
Make modifications so that the divisor is other than 0 when it is executed.
Product Name
MELSEC-Q Series
Series
Q (Q mode)
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
Difference between GX Works2 and GX D...
Error code "2110" in QCPU
How to open a GXW file in GX Works2
Duplicated coil error
Error code "2200" in the universal mo...
page top
OKWave logo