Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22553
  • Release Date : 2018/09/03 17:28
  • Print

Boot operation from the standard ROM

Is the boot operation of universal model QCPU from the standard ROM possible?
Category : 

Answer

The boot operation from the standard ROM is not possible.
The program memory of universal model QCPU is a flash ROM.
Thus, writing in the program memory achieves a ROM operation.
Product Name
MELSEC-Q Series
Series
CPU
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?