FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > USB communication driver
FAQ
USB communication driver
MX Component does not work on a Windows 7-based personal computer with an existing USB communication driver installed.
What are the possible causes?
What are the possible causes?
- Category :
Answer
Is the version of MX Component compatible with Windows 7?
Update the software to the version compatible with Windows 7 and then update the driver.
For the update procedure of the driver, refer to the following technical bulletin.
- FA-A-0091: Products compatible with Windows 7 and precautions for installation
Update the software to the version compatible with Windows 7 and then update the driver.
For the update procedure of the driver, refer to the following technical bulletin.
- FA-A-0091: Products compatible with Windows 7 and precautions for installation
- Product Name
- MELSEC-Q Series
- Series
- Middleware