Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22591
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/21 10:01
  • Print

Resolution provided for Q64AD/Q68ADV/Q68ADI

Does the resolution provided for Q64AD/Q68ADV/Q68ADI become higher if the analog input range is set to "User range setting" and the analog input value corresponding to the maximum digital output value is set to a smaller value using the gain setting?
Category : 

Answer

The maximum resolution for the user range setting does not change.

Product Name
MELSEC-Q Series
Series
A / D Conversion Module
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?