FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > What to do in the case of the error "A default router IP address needs to be set."
FAQ
What to do in the case of the error "A default router IP address needs to be set."
In making the built-in Ethernet port setting for a universal model QCPU module, an error message appears, stating "A default router IP address needs to be set.". Are there any remedies?
- Category :
Answer
When having access bypassing a router, enter only the IP address.The subnet mask pattern is not required to be entered because GX Works2 or GX Developer automatically sets a default subnet mask.
Set the IP address, subnet mask pattern, and default router IP address only when having access via a router.
Set the IP address, subnet mask pattern, and default router IP address only when having access via a router.
- Product Name
- MELSEC-Q Series
- Series
- CPU