FAQ


FAQAbout Products
 
 - FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Error code "2200" in the universal model QCPU
FAQ
Error code "2200" in the universal model QCPU
      The error code "2200" has occurred in a universal model QCPU module. Are there any remedies?
    
  - Category :
Answer
    The error code "2200" is "MISSING PARA.". 
The cause of the error is that a parameter file does not exist in all drives where parameters will be valid.
As a remedy, write a parameter file into a PLC drive to be valid.
    The cause of the error is that a parameter file does not exist in all drives where parameters will be valid.
As a remedy, write a parameter file into a PLC drive to be valid.
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)