Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22744
  • Release Date : 2018/09/03 17:29
  • Print

NTP support by the SNTP function of LCPU with built-in Ethernet port

Is it possible to use a personal computer NTP server as an SNTP server for the time setting function (SNTP client) via the built-in Ethernet port in the L series CPU?
Category : 

Answer

NTP and SNTP are compatible. Therefore, an NTP server can be used for clock setting.
Product Name
MELSEC-L Series
Series
L Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?