Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22768
  • Release Date : 2018/09/03 17:30
  • Print

Compliance with SEMI-F47 for L series power supply module

How do I comply with SEMI-F47 when using the L series power supply module?
Category : 

Answer

Use the following power supply module with an input power of 200 VAC for compliance with SEMI-F47.
- Power supply module: L61P

With an input power of 100 VAC, supply power via an uninterruptible power supply (UPS) to the programmable controller system for compliance with SEMI-F47. Use an online UPS with voltage distortion of 5% or less.
(1) Connectable online Mitsubishi UPS products
- FREQUPS-V series

(2) Connectable Mitsubishi UPS products other than online types
- FREQUPS-A series
- FREQUPS-F series (serial number P or later)
Product Name
MELSEC-L Series
Series
Power Supply
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?