Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22769
  • Release Date : 2018/09/03 17:30
  • Print

Versions of built-in Ethernet port LCPU compatible with SNTP function

I would like to use the time setting function (SNTP client) of the L series CPU with built-in Ethernet port to synchronize clocks. Are there any restrictions on the model or version of CPU?
Category : 

Answer

The initial version and subsequent versions of L series CPU support the SNTP function.
Product Name
MELSEC-L Series
Series
L Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?