FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > FNC connector pin layout in L series I/O module and Q series I/O module
FAQ
FNC connector pin layout in L series I/O module and Q series I/O module
Do LX41C4, LX42C4, LY41NT1P, and LY42NT1P have the same pin layout as QX41 and 42, and QY41P and 42P?
- Category :
Answer
Yes. They have the same pin layout.
- Product Name
- MELSEC-L Series
- Series
- L Series
May I have your opinion?
Related FAQ
- Maximum number of connectable modules to LCPU when it is not extended
- Conversion speed of L60AD4
- Storing the data logging setting to an SD memory card in LCPU
- Behavior of sequence program in event of momentary power failure in LCPU
- Simultaneous broadcast reception setting for built-in Ethernet port LCPU