FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Support for Q series RS-232 cable
FAQ
Support for Q series RS-232 cable
Can I use a Q series RS-232 cable with the L series RS-232 adapter?
- Category :
Answer
Yes.
- Product Name
- MELSEC-L Series
- Series
- CPU
May I have your opinion?
Related FAQ
- Difference between standard inputs A06 to B11 and high-speed inputs A12 to B20 of LCPU built-in I/O function
- Use of an A-compatible 1E frame for the built-in Ethernet port of LCPU
- Restriction on the use of CPU when branch module and extension module are used
- Number of data sampling points in LCPU logging function
- Loop disconnection detection function and heater disconnection detection function of temperature control module