Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22846
  • Release Date : 2018/09/03 17:30
  • Print

Automatically assigned devices in GX Works2

Are automatically assigned devices in GX Works2 assigned from the last device, whether they are for global labels or local labels?
Category : 

Answer

Yes.
Beginning with the device in the "Device/Label Automatic-Assign Setting" window, devices are assigned in descending order (from the greatest device number) within the set range of devices.
When there are both global labels and local labels, the devices are first assigned to the global labels and subsequently assigned to the local labels.
Product Name
Engineering Software
Series
Software Package (GPP function)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?