FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Behavior of special relay in offline simulation
FAQ
Behavior of special relay in offline simulation
In GX Simulator, SM410 is still OFF even after an offline simulation starts.How can I turn ON/OFF SM410?
- Category :
Answer
The constant scan initial value of GX Simulator is 100 ms. Thus, the value of SM410(0.1sec. clock) is OFF in each scan.
To turn ON/OFF SM410, set the constant scan value to other than integral multiples of the clock time.
Set the constant scan setting value in [PLC Parameter] -> [PLC RAS setting] tab.
To turn ON/OFF SM410, set the constant scan value to other than integral multiples of the clock time.
Set the constant scan setting value in [PLC Parameter] -> [PLC RAS setting] tab.
- Product Name
- Engineering Software
- Series
- Software Package (other functions)