Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22941
  • Release Date : 2018/09/03 17:30
  • Update : 2018/09/25 09:58
  • Print

Displaying comments in GX Works2

How can I display comments in the ladder editor (circuit) of GX Works2?
Category : 

Answer

Select [View] -> [Comment] from the menu to display comments.
You can display local comments with the following procedure.

(1) Select [Tool] -> [Options] from the menu to open the Option window.
(2) Select [Program Editor] -> [All Editors] -> [Device Comment] from the tree on the left of the window.
(3) In Reference/Reflection Target for Device Comment, select global comments 
     or local comments as the device comments of each program.
Product Name
Engineering Software
Series
Software Package (GPP function)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?